Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
DSP Blackfin STAMP BSP Slide 9

The start file is the program that is executed before the main and simple applications. C libraries are also needed. These are used to interface to the kernel and the system calls. These need to be specified in the example. gcc will be used to turn off the default start files, trigger a special flat file object linker, and specify where the start file, the object, the test code, and the libraries are. The Blackfin has an assembler syntax called arithmetic notation, which allows users to see what the assembler is doing in an understandable format. The assembly output can be seen during testing or by specifying a -S compiler option. That will give the assembler the corresponding C code which can then relate the two.

PTM Published on: 2006-01-20