Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
DSP Blackfin STAMP BSP Slide 26

The stamp system has uboot version 1.1.3 with an Ethernet interface. It has TFTP or serial image loading, Flash management, elf file support, and the ability to automate the boot. There is also a set of example peripheral drivers to help writing device drivers. Instructions, data cache management and DMA interfaces are also included.

PTM Published on: 2006-01-20