Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
DSP Blackfin STAMP BSP Slide 7

The tools needed are a compiler, an assembler, and a linker. The compiler generates assembler output from a C input. The assembler then translates that into machine code from assembler sources and produces an output that can be linked together into one or many objects into a final output for deployment on the system. There are additional tools which allow users to copy, relocate, and manipulate the elf objects.

PTM Published on: 2006-01-20