Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
DSP Blackfin STAMP BSP Slide 14

Blackfin is using the 2.6.12 kernel. In the 2.6 series the uClinux or the [MMU-less] Linux options are actually built-in and integrated into the kernel. The key features in the 2.6 kernel include a better scheduler, native thread support built into the kernel, access large memory, an I/O scheduler and the start of power management and wireless integration. It’s important, when working with an open-source software package, to keep the original source and keep the changes as patches.

PTM Published on: 2006-01-20