Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
DSP Blackfin STAMP BSP Slide 3

This diagram is used to illustrate the 5 processor P’s: Price, Power, Performance, Peripherals, and Penguins. These domains are all well supported by the Blackfin processor. All Blackfin Processors offer fundamental benefits to the system designer which include high-performance signal processing and efficient control processing capability enabling a variety of new markets and applications. Dynamic Power Management (DPM) enables the system designer to specifically tailor the device power consumption profile to the end system requirements. Also included is an easy to use mixed 16-/32-bit Instruction Set Architecture and development tool suite ensuring that product development time is minimized. The Blackfin is also supported by a set of open source tools (uClinux kernel, GNU toolchain U-boot). The source for each is freely available on http://blackfin.uclinux.org, covered by a GPL or other OSI approved license. Many people are using the combination of Open Source and the Blackfin processor to decrease development effort, and add new and innovative features to their designs.

PTM Published on: 2006-01-20