Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
DSP Blackfin STAMP BSP Slide 17

Distribution is a development environment. It contains the kernel, the libraries and the user applications. It also contains a mechanism for configuring the whole system using a graphical environment and a saved configuration for preset targets. Most importantly, it has a structured set of make files which provides the one-stop build environment. Typing "make" in the source directory will capture the target architecture and system and produce an image specifically for that target. It encapsulates all the configuration options. A graphical configuration mechanism manages how to invoke the compiler, how to run the linker, and the include files. It generates a root file system which the kernel needs to run, and the production of an image to transfer to the target system. The uClinux distribution is designed to switch architectures and projects easily, so by selecting a different root source of configuration, you can compile for a different target.

PTM Published on: 2006-01-20