Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
DSP Blackfin STAMP BSP Slide 13

There is also a Blackfin port of coLinux available. coLinux is short for “cooperative Linux” and it is a port of the Linux kernel that allows it to run cooperatively alongside another operating system on a single machine. Cooperative Linux is the first working free and open source method for optimally running Linux on Microsoft Windows natively. It provides all the benefits of a UNIX system without leaving the Windows environment. coLinux tends to be slower than native Linux® and the time to make builds can add up over time. It is helpful when it is necessary to remain in a Windows environment. Step-by-step directions on how to install coLinux for the Blackfin can be found on the following website: http://docs.blackfin.uclinux.org/doku.php?id=colinux. For further information on colinux, go to http://www.colinux.org/.

PTM Published on: 2006-01-20