Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
DSP Blackfin STAMP BSP Slide 21

Next is the boot loader. Analog Devices has the source at http://uboot.sourceforge.net, under active development. They can be located by going to https://blackfin.uclinux.org/doku.php site to find patches for the boot loader. The boot loader can understand environment variables, do a serial download via Ethernet, or it can extract an image from its own flash memory. It has flash management capability as well. If an image has to be put in the flash memory, something must be done to it to make uboot understand. It needs to be wrapped in a header and the "makeimage" command there. An example has been extracted which is used to take the linux.dxe elf image and wrap it such that the boot loader can understand it.

PTM Published on: 2006-01-20