At higher voltages the capacitance retention is still more than 90% at –55°C and 120Hz but there is more fall off at higher frequencies. Notice however that the 5% capacitance retention at 10kHz is 50µF - a lot of capacitance.
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
At higher voltages the capacitance retention is still more than 90% at –55°C and 120Hz but there is more fall off at higher frequencies. Notice however that the 5% capacitance retention at 10kHz is 50µF - a lot of capacitance.
Obrigado!
Fique de olho em sua caixa de entrada para notícias e atualizações da DigiKey!
Digite um endereço de e-mail
Por favor, marque a caixa de seleção