STM32MP1 Primer – Day 3
The STM32MP157x dual core design pairs up a powerful Linux-enabled Cortex-A7 MPU with a speedy Cortex-M4 MCU. At first glance one would think that the Cortex-M4 is a luxury as the Cortex-A7 is fully capable of handling complex applications without any help from the Cortex-M4. However, the Cortex-A7 running under the control of a Linux kernel is not very good when it comes to precise millisecond and microsecond timing within the application. On the other hand, the Cortex-M4 can turn on a microsecond. An ideal situation would exist if we could run our heavy application loads using the Cortex-A7 and use the Cortex-M4 as a real-time coprocessor for the tasks that require more accurate time resolution. The application we will build in today's lecture will enable an interprocessor communications link between the Cortex-A7 and the Cortex-M4 cores.
Microprocessors
| Imagem | Número de peça do fabricante | Descrição | Available Quantity | Preço | Ver detalhes | |
|---|---|---|---|---|---|---|
![]() | ![]() | STM32MP157FAC1 | IC MPU STM32MP1 800MHZ 361TFBGA | 2411 - Immediate | $17.16 | Ver detalhes |
![]() | ![]() | STM32MP157CAA3 | IC MPU STM32MP1 650MHZ 448LFBGA | 199 - Immediate | $17.97 | Ver detalhes |
![]() | ![]() | STM32MP151CAA3 | IC MPU STM32MP1 650MHZ 448LFBGA | 201 - Immediate | $13.67 | Ver detalhes |
![]() | ![]() | STM32MP135FAE7 | 32-BIT ARM CORTEX-A7 900MHZ MPU | 396 - Immediate | $11.85 | Ver detalhes |
![]() | ![]() | STM32MP153CAA3 | IC MPU STM32MP1 650MHZ 448LFBGA | 0 - Immediate | $16.29 | Ver detalhes |
STMicroelectronics Embedded MCU, DSP Evaluation Boards
| Imagem | Número de peça do fabricante | Descrição | Available Quantity | Preço | Ver detalhes | |
|---|---|---|---|---|---|---|
![]() | ![]() | STM32MP157D-DK1 | DISCOVERY STM32MP157D EVAL BRD | 20 - Immediate | $159.50 | Ver detalhes |
![]() | ![]() | STM32MP135F-DK | DISCOVERY KIT WITH STM32MP135F M | 20 - Immediate | $177.05 | Ver detalhes |
![]() | ![]() | STM32MP157F-DK2 | DISCOVERY STM32MP157F CRYPTO BRD | 220 - Immediate | $203.00 | Ver detalhes |
![]() | ![]() | STM32MP157F-EV1 | STM32MP157F CRYPTO EVAL BRD | 20 - Immediate | $503.66 | Ver detalhes |
![]() | ![]() | STM32MP157D-EV1 | STM32MP157D EVAL BRD | 2 - Immediate | $425.00 | Ver detalhes |
![]() | ![]() | STM32MP157A-DK1 | DISCOVERY STM32MP157A EVAL BRD | 0 - Immediate | $70.15 | Ver detalhes |
![]() | ![]() | STM32MP157C-DK2 | DISCOVERY STM32MP157C CRYPTO BRD | 0 - Immediate | $99.69 | Ver detalhes |
![]() | ![]() | STM32MP157C-EV1 | STM32MP157C CRYPTO EVAL BRD | 0 - Immediate | $399.00 | Ver detalhes |
![]() | ![]() | MIKROE-4122 | PI 4 CLICK SHIELD | 28 - Immediate | $30.00 | Ver detalhes |