VideoLibrary

STM32MP1 Primer – Day 5

This week's lectures have thus far taught us how to configure and use the STM32MP157x GPIO that is common to both the Cortex-A7 and Cortex-M4 cores. We have also experienced the sensation of sitting on the I2C and USART limbs of the STM32MP157x device tree. Today we will climb the device tree one more time. There's a limb dedicated to providing leaves and branches that enable the STM32MP157x's OpenSTLinux-based SPI peripherals. The configuration of the SPI peripherals within the device tree is quite unique and must be understood thoroughly to enable any of the STM32MP157x SPI peripherals. Today's lecture will be built upon a couple of projects. First, we will code an embedded Linux driver for the popular SSD1306-based display. The SSD1306 is heavily data output-only oriented. The second project will assemble a number of embedded Linux routines designed to drive a MCP23S17 16-bit Expander with Serial Interface. The MCP23S17 driver will contain input capture algorithms as well as standard SPI output routines. Just as we have done all week, we will utilize STM32CubeMX and STM32CubeIDE to generate the device tree assign SPI peripheral GPIO pins and compile our SPI driver source code. The SPI driver code will be capable of interfacing to SPI hardware on the STM32MP157x discovery board's Raspberry Pi 4 and Arduino physical interfaces.

1/29/2025 8:59:48 PM

Microprocessors

ImagemNúmero de peça do fabricanteDescriçãoAvailable QuantityPreçoVer detalhes
IC MPU STM32MP1 800MHZ 361TFBGASTM32MP157FAC1IC MPU STM32MP1 800MHZ 361TFBGA2411 - Immediate$17.16Ver detalhes
IC MPU STM32MP1 650MHZ 448LFBGASTM32MP157CAA3IC MPU STM32MP1 650MHZ 448LFBGA199 - Immediate$17.97Ver detalhes
IC MPU STM32MP1 650MHZ 448LFBGASTM32MP151CAA3IC MPU STM32MP1 650MHZ 448LFBGA201 - Immediate$13.67Ver detalhes
32-BIT ARM CORTEX-A7 900MHZ MPUSTM32MP135FAE732-BIT ARM CORTEX-A7 900MHZ MPU396 - Immediate$11.85Ver detalhes
IC MPU STM32MP1 650MHZ 448LFBGASTM32MP153CAA3IC MPU STM32MP1 650MHZ 448LFBGA0 - Immediate$16.29Ver detalhes

STMicroelectronics Embedded MCU, DSP Evaluation Boards

ImagemNúmero de peça do fabricanteDescriçãoAvailable QuantityPreçoVer detalhes
DISCOVERY STM32MP157D EVAL BRDSTM32MP157D-DK1DISCOVERY STM32MP157D EVAL BRD20 - Immediate$159.50Ver detalhes
DISCOVERY KIT WITH STM32MP135F MSTM32MP135F-DKDISCOVERY KIT WITH STM32MP135F M20 - Immediate$177.05Ver detalhes
DISCOVERY STM32MP157F CRYPTO BRDSTM32MP157F-DK2DISCOVERY STM32MP157F CRYPTO BRD182 - Immediate$203.00Ver detalhes
STM32MP157F CRYPTO EVAL BRDSTM32MP157F-EV1STM32MP157F CRYPTO EVAL BRD20 - Immediate$503.66Ver detalhes
STM32MP157D EVAL BRDSTM32MP157D-EV1STM32MP157D EVAL BRD2 - Immediate$425.00Ver detalhes
PI 4 CLICK SHIELDMIKROE-4122PI 4 CLICK SHIELD28 - Immediate$30.00Ver detalhes
DISCOVERY STM32MP157A EVAL BRDSTM32MP157A-DK1DISCOVERY STM32MP157A EVAL BRD0 - Immediate$70.15Ver detalhes
DISCOVERY STM32MP157C CRYPTO BRDSTM32MP157C-DK2DISCOVERY STM32MP157C CRYPTO BRD0 - Immediate$99.69Ver detalhes
STM32MP157C CRYPTO EVAL BRDSTM32MP157C-EV1STM32MP157C CRYPTO EVAL BRD0 - Immediate$399.00Ver detalhes