VideoLibrary

IoT Device Prototyping with STMicroelectronics Nucleo Development Boards – Day 5

STMicroelectronics provides a set of functions packaged as a BSP (Board Support Package) that is designed to support the X-NUCLEO-GFX01M1 Display Expansion. If you browse the functions contained within the BSP you will note that all of the BSP functions reference the ILI9341 TFT driver SOC. If your application requires the storage and retrieval of pretty pictures the X-NUCLEO-GFX01M1 comes loaded with an MX25L6433Fa 64-Mbit SPI NOR Flash device that is also supported by the BSP. The X-NUCLEO-GFX01M1 interfaces to the NUCLEO-G071RB's on-board STM32G071RB microcontroller via the NUCLEO-G071RB's MORPHO headers. Since the X-NUCLEO-GFX01M1's display is not touch-enabled interaction between the user the display and the application can be enabled by coding in the GPIO pins that are attached to the X-NUCLEO-GFX01M1's on-board joystick. The goal of today's lecture is to gain an understanding of how the X-NUCLEO-GFX01M1 BSP functions work and apply our new-found knowledge in the form of a joystick-enabled wireless remote control IoT application.

1/30/2025 6:41:25 PM

Evaluation Boards

ImagemNúmero de peça do fabricanteDescriçãoAvailable QuantityPreçoVer detalhes
NUCLEO-64 STM32G071RB EVAL BRDNUCLEO-G071RBNUCLEO-64 STM32G071RB EVAL BRD649 - Immediate$20.13Ver detalhes
NUCLEO-144 STM32U575ZI EVAL BRDNUCLEO-U575ZI-QNUCLEO-144 STM32U575ZI EVAL BRD788 - Immediate$26.64Ver detalhes
NANO LR CLICKMIKROE-4514NANO LR CLICK1 - Immediate$65.00Ver detalhes
MICROSD CLICKMIKROE-924MICROSD CLICK65 - Immediate$19.00Ver detalhes

Microcontrollers

ImagemNúmero de peça do fabricanteDescriçãoAvailable QuantityPreçoVer detalhes
IC MCU 32BIT 128KB FLSH 28UFQFPNSTM32G071GBU6TRIC MCU 32BIT 128KB FLSH 28UFQFPN585 - Immediate$2.85Ver detalhes
IC MCU 32BIT 128KB FLSH 28UFQFPNSTM32G071GBU6IC MCU 32BIT 128KB FLSH 28UFQFPN3793 - Immediate$2.85Ver detalhes
IC MCU 32BIT 128KB FLSH 48UFQFPNSTM32G071CBU6IC MCU 32BIT 128KB FLSH 48UFQFPN1011 - Immediate$3.22Ver detalhes
IC MCU 32BIT 128KB FLASH 48LQFPSTM32G071CBT6IC MCU 32BIT 128KB FLASH 48LQFP2070 - Immediate$3.35Ver detalhes
IC MCU 32BIT 128KB FLASH 48LQFPSTM32G071CBT6TRIC MCU 32BIT 128KB FLASH 48LQFP2188 - Immediate$3.37Ver detalhes