When double clicking on the project folder in the project navigator window, one can see that all of the DriverLib files are included in the DriverLib folder. The project is also prepopulated with a main .c file that includes the necessary header files. Change the project properties to select the FR5969 device and the project is now enabled with DriverLib.