In this generic guideline table, a direct relation is presented between the most common power rails and the 10% and 20% derating levels, defined by the series to be used and the mission profile of the application in terms of temperature.
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
In this generic guideline table, a direct relation is presented between the most common power rails and the 10% and 20% derating levels, defined by the series to be used and the mission profile of the application in terms of temperature.
Obrigado!
Fique de olho em sua caixa de entrada para notícias e atualizações da DigiKey!
Digite um endereço de e-mail
Por favor, marque a caixa de seleção