Dynamic testing means that the electronic load can be switched between two set parameters according to the set rules. IT8500G+’s dynamic mode could test up to 20kHz. This function is used to test the dynamic characteristics of power supplies.
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
Dynamic testing means that the electronic load can be switched between two set parameters according to the set rules. IT8500G+’s dynamic mode could test up to 20kHz. This function is used to test the dynamic characteristics of power supplies.