DACs Part 4 Buffering

Data Converters- Five Things to Know About DACs Part 4: Buffering

Analog Devices Inc

So far in this series, resolution and accuracy, total unadjusted error, and output noise have been covered. This module will now take a look at the buffering of the DAC. It is split into two sections: buffering of the reference input pin, and buffering of the output. Both sections will discuss some of the technologies that require buffering as well as some instances where buffering is not necessary. Additionally, some tips on selecting buffers will be presented at the end of this module.

Digital to Analog Converters (DAC)

ImagemNúmero de peça do fabricanteDescriçãoAvailable QuantityPreço
IC DAC 12BIT 16-CERDIP5962-9320401MEAIC DAC 12BIT 16-CERDIP0 - ImmediateSee Page for PricingVer detalhes
IC DAC 12BIT SOT-23-8AD5620BRJZ-1500RL7IC DAC 12BIT SOT-23-8696 - Immediate$7.09Ver detalhes
IC DAC 12BIT SOT-23-8AD5620BRJZ-2500RL7IC DAC 12BIT SOT-23-81084 - Immediate$7.09Ver detalhes
IC DAC 8BIT 16-TSSOPAD5308ARUZ-REEL7IC DAC 8BIT 16-TSSOP90 - Immediate$9.13Ver detalhes
IC DAC 12BIT SC-70-6AD5621BKSZ-500RL7IC DAC 12BIT SC-70-61617 - Immediate$3.73Ver detalhes
IC DAC 12BIT SC-70-6AD5621BKSZ-REEL7IC DAC 12BIT SC-70-69457 - Immediate$3.73Ver detalhes
IC DAC 8BIT SOT-23-6AD5300BRTZ-REEL7IC DAC 8BIT SOT-23-65330 - Immediate$5.67Ver detalhes
IC DAC 8BIT SOT-23-6AD5300WBRTZ-RL7IC DAC 8BIT SOT-23-63000 - Immediate$6.43Ver detalhes
IC DAC 18BIT 32-BBDIP-HAD1139JIC DAC 18BIT 32-BBDIP-H0 - ImmediateSee Page for PricingVer detalhes
IC DAC 18BIT 32-BBDIP-HAD1139KIC DAC 18BIT 32-BBDIP-H0 - ImmediateSee Page for PricingVer detalhes

ADCs/DACs - Special Purpose

ImagemNúmero de peça do fabricanteDescriçãoAvailable QuantityPreço
IC DAS/ADC/DAC SPECIAL 16-SOICAD421BRZIC DAS/ADC/DAC SPECIAL 16-SOIC4603 - Immediate$22.96Ver detalhes
IC DAS/ADC/DAC SPECIAL 16-PDIPAD421BNZIC DAS/ADC/DAC SPECIAL 16-PDIP125 - Immediate$25.72Ver detalhes
IC DAS/ADC/DAC SPECIAL 16-SOICAD421BRZRLIC DAS/ADC/DAC SPECIAL 16-SOIC4363 - Immediate$22.96Ver detalhes
IC DAS/ADC/DAC SPECIAL 16-SOICAD421BRZRL7IC DAS/ADC/DAC SPECIAL 16-SOIC1249 - Immediate$22.96Ver detalhes
IC DAS/ADC/DAC SPECIAL 16-SOICAD421BRIC DAS/ADC/DAC SPECIAL 16-SOIC0 - ImmediateSee Page for PricingVer detalhes
IC DAS/ADC/DAC SPECIAL 16-PDIPAD421BNIC DAS/ADC/DAC SPECIAL 16-PDIP0 - ImmediateSee Page for PricingVer detalhes
PTM Published on: 2012-10-25