Maker.io main logo

Remote Control Tree Ornament with Circuit Playground Express

54

2017-12-27 | By Adafruit Industries

License: See Original Project Circuit Playground

Courtesy of Adafruit

Guide by John Park

Overview

Have you put up with non-interactive, regular, old, low-tech tree ornaments for too long? Yes you have! But, this is where things change! It's time to build your own Remote Control Tree Ornament with Circuit Playground Express!!

The Circuit Playground Express (CPX) has a built in infrared (IR) sensor, and it's very simple to decode the signals using CircuitPython, thanks to the Adafruit IR Remote library.

We'll program the CPX to read IR blasts from the mini remote control, and use these commands to change the bright, beautiful NeoPixels. Plus, we'll defuse the light and dress it up with an inexpensive hobby store ornament and festive puff balls!

1 x  Circuit Playground Express - Awesome microcontroller with CircuitPython

1 x  Mini Remote Control - IR remote with NEC encoding

1 x  Battery Holder w On/Off switch - 3 x AAA battery holder

1 x  Alkaline AAA batteries

1 x  USB Cable - USB A to USB Micro - 3 ft.

Or, optionally, to get most of those parts in a single pack, and then just add the remote!

1 x  Circuit Playground Express Base Kit - Includes CPX, battery pack and batteries, USB cable, and storage box

Materials

In addition to the electronics, you'll need:

  • Clear 4" ball ornament from a hobby store that opens into two halves

  • White iridescent pom poms

  • Ribbon or tree hanger hook

White iridescent pom poms

Code the Circuit Playground Express

You'll program your ornament to change colors based on the numbered buttons on the IR mini remote control by using CircuitPython.

Get Ready!

First, make sure you're up and running by following these steps:

Library Bundle

  • There's one extra library to install for this project, that'll let you use the IR remote -- download the Adafruit IRRemote library and place it in the lib folder on your CircuitPython

Lighting up the NeoPixel ring in different colors is simple to do on the Circuit Playground Express using CircuitPython. In fact, it only takes a single line of code to make them all bright red: pixels.fill(255, 0, 0) will do the trick in the case of our program!

To control which colors we see, we can use can use the IR remote control along with IR library that makes it easy to decode the IR commands.

IR commands are actually messages that are sent by the remote when it blinks its infrared light rapidly with very precise timing and duration. It's a little bit like Morse code in that sense.

Using its IR sensor, the Circuit Playground Express can decode those messages sent by the remote. For more details on how this works, check out this great IR sensor guide.

So that you don't need to deal with the low level complexities of the decoding process, the Adafruit IRRemote library makes it simple!

Download the Remote Tree Ornament Code

Copy the code below, and paste it into a new text document in your text editor, or in the Mu code editor for CircuitPython.

Copy Code
import adafruit_irremote
import board
import digitalio
import neopixel
import pulseio

pixels = neopixel.NeoPixel(board.NEOPIXEL, 10)

red_led = digitalio.DigitalInOut(board.D13)
red_led.direction = digitalio.Direction.OUTPUT

pulsein = pulseio.PulseIn(board.REMOTEIN, maxlen=120, idle_state=True)
decoder = adafruit_irremote.GenericDecode()

# among others, this example works with the Adafruit mini IR remote:
# https://www.adafruit.com/product/389
# size must match what you are decoding! for NEC use 4
received_code = bytearray(4)

# IR Remote Mapping
'''
 1: [255, 2, 247, 8]
 2: [255, 2, 119, 136]
 3: [255, 2, 183, 72]
 4: [255, 2, 215, 40]
 5: [255, 2, 87, 168]
 6: [255, 2, 151, 104]
 7: [255, 2, 231, 24]
 8: [255, 2, 103, 152]
 9: [255, 2, 167, 88]
 0: [255, 2, 207, 48]

^ : [255, 2, 95, 160]
v : [255, 2, 79, 176]
> : [255, 2, 175, 80]
< : [255, 2, 239, 16]

Enter: [255, 2, 111, 144]
Setup: [255, 2, 223, 32]
Stop/Mode: [255, 2, 159, 96]
Back: [255, 2, 143, 112]

Vol - : [255, 2, 255, 0]
Vol   : [255, 2, 191, 64]

Play/Pause: [255, 2, 127, 128]
'''

RED = (255, 0, 0)
GREEN = (0, 255, 0)
WHITE = (85, 85, 85)
BLUE = (0, 0, 255)
PINK = (128, 0, 128)
YELLOW = (148, 108, 0)
PURPLE = (200, 0, 55)
TEAL = (0, 200, 100)
ORANGE = (100, 45, 0)
BLACK = (0, 0, 0)

last_command = None

while True:
    red_led.value = False
    try:
        pulses = decoder.read_pulses(pulsein)
    except MemoryError as e:
        print("Memory error: ", e)
        continue
    red_led.value = True
    print("Heard", len(pulses), "Pulses:", pulses)
    command = None
    try:
        code = decoder.decode_bits(pulses, debug=False)
        if len(code) > 3:
            command = code[2]
        print("Decoded:", code)
    except adafruit_irremote.IRNECRepeatException:  # unusual short code!
        print("NEC repeat!")
        command = last_command
    except adafruit_irremote.IRDecodeException as e:     # failed to decode
        print("Failed to decode:", e)
    except MemoryError as e:
        print("Memory error: ", e)

    if not command:
        continue
    last_command = command

    print("----------------------------")
    red_led.value = False

    if command == 247:  # IR button 1
        pixels.fill(RED)
    elif command == 119:  # 2
        pixels.fill(GREEN)
    elif command == 183:  # 3
        pixels.fill(WHITE)
    elif command == 215:  # 4
        pixels.fill(BLUE)
    elif command == 87:  # 5
        pixels.fill(PINK)
    elif command == 151:  # 6
        pixels.fill(YELLOW)
    elif command == 231:  # 7
        pixels.fill(PURPLE)
    elif command == 103:  # 8
        pixels.fill(TEAL)
    elif command == 167:  # 9
        pixels.fill(ORANGE)
    elif command == 207:
        pixels.fill(BLACK)  # 0/10 

Now, save the code onto your Circuit Playground Express as main.py

The board will restart once the code has been saved. Now, point the remote at the board and press any number button 1-9. See how the lights change color depending on the button!

Code Tour

Let's have a look at how the code works.

First, we import a few libraries that give us easy commands to use for more complex tasks.

Copy Code
import adafruit_irremote
import board
import digitalio
import neopixel
import pulseio

Next, we'll do a bit of setup, creating the NeoPixel object named pixels, and the on-board indicator LED called red_led.

Copy Code
pixels = neopixel.NeoPixel(board.NEOPIXEL, 10)

red_led = digitalio.DigitalInOut(board.D13)
red_led.direction = digitalio.Direction.OUTPUT

To prepare the IR pulse detection and decoding, we'll initialize these objects:

Copy Code
pulsein = pulseio.PulseIn(board.REMOTEIN, maxlen=120, idle_state=True)
decoder = adafruit_irremote.GenericDecode()

Next, we'll create a variable to store the decoded message number list:

Copy Code
received_code = bytearray(4)

Messages

The messages will be sets of four numbers. Here's a list of which buttons correlate to these messages. We'll use this later in the code to know which button has been pressed.

Copy Code
# IR Remote Mapping
'''
 1: [255, 2, 247, 8]
 2: [255, 2, 119, 136]
 3: [255, 2, 183, 72]
 4: [255, 2, 215, 40]
 5: [255, 2, 87, 168]
 6: [255, 2, 151, 104]
 7: [255, 2, 231, 24]
 8: [255, 2, 103, 152]
 9: [255, 2, 167, 88]
 0: [255, 2, 207, 48]

^ : [255, 2, 95, 160]
v : [255, 2, 79, 176]
> : [255, 2, 175, 80]
< : [255, 2, 239, 16]

Enter: [255, 2, 111, 144]
Setup: [255, 2, 223, 32]
Stop/Mode: [255, 2, 159, 96]
Back: [255, 2, 143, 112]

Vol - : [255, 2, 255, 0]
Vol   : [255, 2, 191, 64]

Play/Pause: [255, 2, 127, 128]
'''

Note

Color Names

Next, we'll create a few variables that make it easier to call out colors by name. The colors of the NeoPixels are described with red, green, and blue values from 0-255.

Copy Code
RED = (255, 0, 0)
GREEN = (0, 255, 0)
WHITE = (85, 85, 85)
BLUE = (0, 0, 255)
PINK = (128, 0, 128)
YELLOW = (148, 108, 0)
PURPLE = (200, 0, 55)
TEAL = (0, 200, 100)
ORANGE = (100, 45, 0)
BLACK = (0, 0, 0)

We'll also create a variable to store the value of the last command decoded from the remote, so that we can compare commands to the previous one to know if anything has to change.

Copy Code
last_command = None

Main Loop

Now we get to the main loop that runs over and over after the line:

while True:

The first thing we do is turn the red LED off. This way, when an IR command is received later, the LED can be turned on to indicate this. In the absence of that, the LED will turn back off.

red_led.value = False

This next section is where the IR pulses are detected, and then tested to see if they conform to the expected protocol. If so, the decoded pulses are turned into a message we can use.

Copy Code
    try:
        pulses = decoder.read_pulses(pulsein)
    except MemoryError as e:
        print("Memory error: ", e)
        continue
    red_led.value = True
    print("Heard", len(pulses), "Pulses:", pulses)
    command = None
    try:
        code = decoder.decode_bits(pulses, debug=False)
        if len(code) > 3:
            command = code[2]
        print("Decoded:", code)
    except adafruit_irremote.IRNECRepeatException:  # unusual short code!
        print("NEC repeat!")
        command = last_command
    except adafruit_irremote.IRDecodeException as e:     # failed to decode
        print("Failed to decode:", e)
    except MemoryError as e:
        print("Memory error: ", e)

    if not command:
        continue
    last_command = command

    print("----------------------------")
    red_led.value = False

Color Commands

Lastly, we'll check the received commands against a list -- if the command corresponds to one of them, the code to change the NeoPixel colors is run.

Copy Code
    if command == 247:  # IR button 1
        pixels.fill(RED)
    elif command == 119:  # 2
        pixels.fill(GREEN)
    elif command == 183:  # 3
        pixels.fill(WHITE)
    elif command == 215:  # 4
        pixels.fill(BLUE)
    elif command == 87:  # 5
        pixels.fill(PINK)
    elif command == 151:  # 6
        pixels.fill(YELLOW)
    elif command == 231:  # 7
        pixels.fill(PURPLE)
    elif command == 103:  # 8
        pixels.fill(TEAL)
    elif command == 167:  # 9
        pixels.fill(ORANGE)
    elif command == 207:
        pixels.fill(BLACK)  # 0/10 

Next, we'll build the ornament and use it!

Assemble and Use the Ornament

Fill the Ornament

First, you'll want to tie on the hanging ribbon or hook, and separate the two halves of the clear ornament ball.

Tie hanging ribbon

Next, fill one half with the pom poms. They will look festive, and help to diffuse the strong glow of the NeoPixels on the Circuit Playground Express.

Fill 1/2 with pom poms

Plug the battery pack's JST cable into the Circuit Playground Express, and then turn on the on switch.

Battery pack cable into Circuit Playground Express

Place the CPX and battery pack on top of the pom poms. Looks comfy!

Battery pack on top of pom poms

Now, close up the ornament. It's ready for testing with the remote, and then for hanging on the tree!

Close the ornament

Ready to test

Use the Remote

The IR signal needs to make it to the IR sensor on the CPX, so you may need to try it from different angles. It has the benefit of bouncing off of lots of surfaces, so it isn't hard to make it work from nearby. Without a direct line of sight, it's harder to control it from great distances, but definitely possible!

Use the remote 1

Use the remote 2

Try pressing the different number keys on the remote to see the different colors!

Press different number keys for color 1

Press different number keys for color 2

Now, you may hang it on the tree with care! When it's not in use you can press 0 to turn off the NeoPixels which will preserve battery life. You can also open the ornament to flip off the switch for total energy savings.

Enjoy your festive ornament!

Festive ornament

N.º de peça do fabricante 3333
CIRCUIT PLAYGROUND EXPRESS
Adafruit Industries LLC
$ 24,95
View More Details
N.º de peça do fabricante 1816
LED CBI 5X1.74MM 10SEG WHT VERT
Adafruit Industries LLC
N.º de peça do fabricante IP-USB1(C10)S-RW
CABLE A PLUG TO MCR B PLUG 3.28'
Phihong USA
N.º de peça do fabricante 3517
CIRCUIT PLAYGRND EXPRSS BASE KIT
Adafruit Industries LLC
$ 30,41
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.