Maker.io main logo

ESP32 WhatsApp Alerts Without a SIM Card

15

2026-05-11 | By Rinme Tom

License: General Public License Arduino

The Espressif Systems ESP32 is a favorite among makers because it combines processing power, Wi-Fi, and Bluetooth in a compact and affordable module. One of the most useful capabilities of an internet-connected microcontroller is sending notifications when something important happens.

In this ESP32 WhatsApp Notification project, we’ll build a simple temperature monitor that sends a WhatsApp alert whenever the temperature exceeds a preset limit. The ESP32 reads data from a DHT11 sensor, connects to Wi-Fi, and sends an HTTPS request to the CircuitDigest Cloud WhatsApp API. The cloud service formats the message and delivers it to your phone using WhatsApp—no SIM card, GSM module, or paid WhatsApp Business account required.

This same technique can be used for motion alarms, water-level warnings, equipment monitoring, and countless other IoT projects.

ESP32 Whatsapp Notification

Why Use WhatsApp for IoT Notifications?

Most people check WhatsApp more often than email or SMS. That makes it a practical notification channel for projects that need to get your attention quickly.

Some examples include:

  • Temperature alerts for server rooms or greenhouses

  • Motion detection and security systems

  • Water tank overflow warnings

  • Battery or power-failure notifications

  • Equipment maintenance reminders

Because the ESP32 sends data over Wi-Fi, the system works anywhere with internet access.

Breadboard connection

How the System Works

The workflow is straightforward:

  1. The ESP32 connects to your Wi-Fi network.

  2. It reads temperature and humidity from the DHT11 sensor.

  3. If the temperature exceeds a threshold (for example, 30°C), the ESP32 builds a JSON message.

  4. The board sends the message securely over HTTPS to CircuitDigest Cloud.

  5. The cloud service verifies your API key and sends the WhatsApp message to your registered number.

The free tier currently supports up to five linked phone numbers and approximately 100 messages per month, which is enough for most personal projects.

Parts Required

Components Used

Wiring the DHT11 to the ESP32

Connect the DHT11 as follows:

  • VCC → 5V

  • GND → GND

  • DATA → GPIO 23

If your sensor module includes a pull-up resistor, no additional components are required.

Circuit Diagram

Create Your Free API Key

To send WhatsApp messages, you’ll need an API key from CircuitDigest Cloud.

  1. Open CircuitDigest Cloud and create a free account.

  2. Navigate to Account → API Key.

  3. Generate a new API key.

  4. Open the WhatsApp Notification API section.

  5. Add and verify the phone numbers that should receive alerts.

Only verified numbers can receive notifications.

Understanding Message Templates

WhatsApp requires pre-approved message templates. Instead of sending raw text, you select a template and provide the variable values.

For example, the threshold_violation_alert template might produce a message like:

Alert from Living Room Temp Node
Parameter: Temperature
Measured Value: 31.5°C
Configured Limit: 30°C
Location: Lab

Your ESP32 only sends the values. The cloud platform assembles the final message.

Cloud

Arduino Code

Install the following libraries from the Arduino IDE Library Manager:

  • DHT sensor library by Adafruit

Then upload this sketch.

Copy Code
#include <WiFi.h>
#include <WiFiClientSecure.h>
#include <DHT.h>

#define DHTPIN 23
#define DHTTYPE DHT11
#define TEMP_LIMIT 30.0
#define COOLDOWN_MS 15000

const char* ssid = "YOUR_WIFI_SSID";
const char* password = "YOUR_WIFI_PASSWORD";
const char* apiKey = "YOUR_API_KEY";

const char* host = "www.circuitdigest.cloud";
const int httpsPort = 443;

DHT dht(DHTPIN, DHTTYPE);
WiFiClientSecure client;

unsigned long lastSentTime = 0;

void connectWiFi() {
  WiFi.begin(ssid, password);
  Serial.print("Connecting to WiFi");

  while (WiFi.status() != WL_CONNECTED) {
    delay(500);
    Serial.print(".");
  }

  Serial.println("\nConnected!");
}

void sendWhatsApp(float temperature) {
  client.setInsecure(); // Skip certificate verification

  if (!client.connect(host, httpsPort)) {
    Serial.println("HTTPS connection failed");
    return;
  }

  String tempString = String(temperature, 1) + "°C";

  String payload =
    "{"
      "\"phone_number\":\"919876543210\","
      "\"template_id\":\"threshold_violation_alert\","
      "\"variables\":{"
        "\"device_name\":\"Living Room Temp Node\","
        "\"parameter\":\"Temperature\","
        "\"measured_value\":\"" + tempString + "\","
        "\"configured_limit\":\"30°C\","
        "\"location\":\"Maker Lab\""
      "}"
    "}";

  String request =
    String("POST /api/v1/whatsapp/send HTTP/1.1\r\n") +
    "Host: " + host + "\r\n" +
    "Content-Type: application/json\r\n" +
    "x-api-key: " + apiKey + "\r\n" +
    "Content-Length: " + payload.length() + "\r\n\r\n" +
    payload;

  client.print(request);

  Serial.println("WhatsApp alert sent.");

  while (client.connected()) {
    String line = client.readStringUntil('\n');
    if (line == "\r") break;
  }

  Serial.println(client.readString());
  client.stop();
}

void setup() {
  Serial.begin(115200);
  dht.begin();
  connectWiFi();
}

void loop() {
  float temperature = dht.readTemperature();

  if (isnan(temperature)) {
    Serial.println("Failed to read sensor.");
    delay(2000);
    return;
  }

  Serial.print("Temperature: ");
  Serial.println(temperature);

  if (temperature >= TEMP_LIMIT &&
      millis() - lastSentTime > COOLDOWN_MS) {
    sendWhatsApp(temperature);
    lastSentTime = millis();
  }

  delay(2000);
}

How the Code Works

The sketch starts by connecting the ESP32 to your Wi-Fi network. Every two seconds, it reads the temperature from the DHT11 sensor.

If the measured temperature exceeds TEMP_LIMIT, the sendWhatsApp() function is called.

That function:

  • Opens a secure HTTPS connection

  • Builds a JSON payload

  • Add your API key to the request header

  • Sends the payload to CircuitDigest Cloud

A cooldown timer prevents repeated alerts when the temperature remains above the threshold.

Upload and Test

  1. Replace the Wi-Fi credentials, API key, and phone number.

  2. Select your ESP32 board in the Arduino IDE.

  3. Upload the sketch.

  4. Open the Serial Monitor at 115200 baud.

  5. Warm the DHT11 sensor with your hand or a heat source.

When the temperature crosses 30°C, a WhatsApp message should appear on your phone within a few seconds.

Real-World Applications

Once you understand this workflow, you can swap the DHT11 for nearly any sensor:

  • PIR sensor for intrusion detection

  • Ultrasonic sensor for tank-level monitoring

  • Soil moisture sensor for irrigation control

  • Voltage sensor for battery alerts

  • Current sensor for equipment diagnostics

The notification logic remains the same.

Troubleshooting Tips

If messages are not delivered:

  • Verify that your API key is valid.

  • Confirm the phone number has been linked and verified.

  • Ensure the ESP32 has internet access.

  • Check the serial monitor for HTTP responses.

  • Confirm the selected template ID is correct.

Expanding the Project

Here are a few ideas to build on this project:

  • Add multiple recipients

  • Include humidity in the message

  • Trigger alerts only during specific hours

  • Log readings to a cloud dashboard

  • Combine with email or SMS notifications

Final Thoughts

This project shows how easy it is to add professional-looking WhatsApp notifications to an ESP32 project. Instead of dealing with GSM hardware or paid APIs, you can send alerts over Wi-Fi using a simple HTTPS request.

Whether you are monitoring a greenhouse, protecting a workshop, or building a home automation system, WhatsApp notifications are an effective way to stay informed in real time.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.