Maker.io main logo

Edge Lit Flower with our Kitronik Tricolour LED Boards

57

2025-07-24 | By Kitronik Maker

License: See Original Project Laser Cutters LEDs / Discrete / Modules

Courtesy of Kitronik

Guide by Kitronik Maker

Create that perfect gift for mum, using one of our Kitronik Tricolour LED Boards. This layered light effect display will look great on the mantel piece.

Grab the file, follow Kev's guide, and make your own. The designs can be personalised and changed in any way you like. Please share pics of your makes with us on social media so that we can share them with all of our customers.

covers_1

What we used:

sign_2

STEP 1 - Sowing the seeds:

Download the supplied DXF file for your laser cutter and then go to town. Etch and cut the stand and the flower elements from their respective acrylic colours.

cuts_3

STEP 2 - Attach the base:

Using the short 6mm M3 countersunk screws attach the board to the base layer and build the rest of the base elements around the board, making sure you have access to the USB connection and the on/off button. Attach the whole base unit together using the 4 12mm M3 pan head screws.

base_4

STEP 3 - Plant the flower:

Drop in the clear etched acrylic pieces, aligning them in the correct notches, corresponding to the red, green, blue lights.

plant_5

STEP 4 - Let there be light:

Plug the USB cable into the board and power supply and switch it on.

light_6

Mum’ll love it!

©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof without Kitronik's prior written consent.

N.º de peça do fabricante 35164
KITRONIK TRICOLOUR LED BOARD
Kitronik Ltd.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.