Maker.io main logo

DIY simple GU81 Tube Hybrid Amplifier (130 watts RMS in A class)

445

2023-06-23 | By Mirko Pavleski

License: General Public License Amplifiers

Tube amplifiers are highly respected by audiophiles for their distinctive sound as well as their esoteric appearance. However, their construction is relatively complex, especially in the part of power supply and output audio transformer. For these reasons, there often are made so-called "Hybrid" audio Amplifiers in which the input preamplifier part is made with Tubes, and the output part is usually made with MOSFET transistors due to their high internal resistance, similar to Tubes. Thus, the distortions of the even harmonics, which are in fact the reason for the colored warm sound of the Tube amplifiers, are amplified by the output transistor stage. But unfortunately, these positive distortions occur most often in the output stage of the Tube amplifiers, so the aforementioned Hybrid amplifiers do not have very similar characteristics to the Tube amplifiers.

 

The amplifier described in this project is also Hybrid but now the case is reversed, and the Tube is used at the output, thus preserving all the positive features of a pure Tube Amplifier. Russian big power pentode (transmitter tube) GU81 is used at the output.

p1

Supposedly this tube in this connection (SE) should bring 130 watts RMS as pure Class A. The circuit was presented by M. Anders(https://maanders.de/ext/elo/index.php?action=view&name=gu81w130&text=true) in 2011, but I could not find any data on whether anyone made it, and if it works well. It is basically very simple and consists of components that can be very easily found, with the exception of the output audio transformer. Luckily, I had such a transformer taken from an old 50 watt Dynacord instrumental amplifier.

p2

In order to simplify the project even more, I used some ready-made modules. In the following, I will describe in more detail the construction of this amplifier. GU81 for heating uses 12 volts 10.5 Amps. For that purpose, the simplest way is to use a cheap PC power supply, and in my case it is power supply from old server PC. To extend the service life of the Tube, a series resistor of 2.2 Ohms / 10 Watts is used, which is bridged after twenty seconds from the moment of activation of the power supply. This avoids the shock of a sudden current impact. The next part is the anode power supply of the tube. For this purpose, a microwave oven transformer is used, which is relatively inexpensive and can be easily obtained.

p3

These transformers are not intended for long-term continuous operation, so it is desirable to use two such transformers to which both the primary and the secondary are connected in series, as shown on the circuit.

p4

In both cases the output voltage is about 2.2 Kilovolts.

USE EXTREME CAUTION AROUND HIGH VOLTAGE! HIGH VOLTAGE CAN CAUSE INJURY OR DEATH

I used one transformer because I only used this amplifier during this presentation. Since it is very difficult to find such a component for very high voltage, I made it as follows: Each branch of the Gertz Bridge consists of 5 series connected diodes of type 1n4007 so that the total breakdown voltage of the equivalent Diode is 5000V which is quite enough for this case.

p5

p6

Voltage filtering is performed with eight serially connected electrolytic capacitors for high voltage of 400 Volts, and on each capacitor is connected а parallel resistor of 470 Kohms, which are used to discharge capacitors after shutdown.

p7

For better quality it is recommended that the total capacitance of these capacitors be higher to avoid noise. The power supply of the amplifier containing the transformers, capacitors and the Gretz bridge is covered with Plexiglas for safety reasons, as there are very high voltages here.

p8

Next is the drive stage for the output Tube which is actually a standard AB-class transistor amplifier. Initially, my idea was to use small and cheap 30W D-Class amplifier with active tone control (on the picture), but unfortunately its outputs are not grounded at all, so in this configuration a lot of unwanted noises appeared at the final signal.

p8

Since the rest of the amplifier was completely ready, I decided to use my old 30W AB-class JVC amplifier to drive the output Tube. For this purpose, you can use any home amplifier with an approximately such output power. Of course, you can use one of the AB-class amplifier modules that can be purchased online, but in that case another power supply would be needed, which complicates the construction. And now comes the most important part, to hear how this amplifier sounds in reality. Unfortunately, I do not have a quality sound box to fully feel the sound coming out of this amplifier so I present only its functionality. Anyway, you could not capture the real sound recorded by my smartphone and then played on YouTube. And finally, a conclusion based on my previous extensive experience in the field of self-construction and listening, mostly on transistor amplifiers.

p9

Generally, it cannot be a high-end device, but it is a very interesting project because it shows how a relatively strong Hybrid Tube output amplifier can be made in a relatively simple way. It can theoretically deliver up to 130 watts of RMS in pure A class. I tested it up to about 50 watts of output power in real conditions, for which power is provided and the output audio transformer. It is very important to tell you that during the hearing tests I did not notice the distortions, at least not such that it would be uncomfortable for the ears. I also listened to it on a larger quality sound box, and I am really satisfied with the sound quality, and I was especially surprised by the large output power that the Tube output can deliver in terms of simplicity. Note that at no input signal, a relatively loud noise is heard coming from the high voltage anode power supply, but the reason for this is primarily the small capacity of the filter capacitors (a total of about 17 microfarads in my case) and the fact that the amplifier is not properly grounded and shielded in a metal box. All in all, this is a very interesting and valuable project. Just imagine what it would look like to make a stereo version in a beautiful box lined with glossy lacquered wood. Let me just mention the visual effect at work when these two Tubes emit a yellowish light and look great. And as a very important note, keep in mind that this circuit is not a toy or a beginner's craft project. Experimenting with it should only be done with well-founded specialist knowledge in the fields of electrical engineering / electronics. This circuit is only intended to show how an enormous power amplifier can be generated with little effort. For safety reasons, the capacitors, transformer, and the bridge rectifier should be housed in a protected housing (wood / plexiglass).

p10

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.