Maker.io main logo

Arduino Proximity Sensor - Activated OLED Smart & Industrial Automation

304

2025-06-04 | By Ron Cutts

License: General Public License Displays Infrared Proximity Real Time Clocks (RTCs) Arduino

Project Description:

A compact and efficient smart display system that uses an IR obstacle sensor to detect motion or presence. When a hand or object is extended towards the sensor, an OLED display automatically turns on, showing useful information such as status updates, sensor readings, or notifications. After 3 seconds of inactivity, the display turns off to conserve power.

Potential Applications:

Smart Home Automation – Display room temperature, security alerts, or appliance statuses only when someone is nearby.

Industrial Use – Hands-free status monitoring in factories, reducing distractions and energy consumption.

Smart Gadgets – Interactive control panels for IoT devices that activate only when needed.

Energy-Saving Display Systems – Reduces power consumption in battery-operated or low-power devices.

Step 1: What You Will Need

What You Will Need

What You Will Need

What You Will Need

What You Will Need

What You Will Need

What You Will Need

  1. Arduino UNO (Or any other Arduino)

  2. Breadboard

  3. OLED Display I2C

  4. Obstacle avoidance sensor

  5. Jumper wires

  6. Visuino program: Download Visuino

Step 2: The Circuit

The Circuit

  1. Connect Obstacle avoidance sensor pin[VCC] to Arduino pin[5V]

  2. Connect Obstacle avoidance sensor pin[GND] to Arduino pin[GND]

  3. Connect Obstacle avoidance sensor pin[D0] to Arduino digital pin[2]

  4. Connect OLED Display pin [SCL] to Arduino pin [SCL]

  5. Connect OLED Display pin [SDA] to Arduino pin [SDA]

  6. Connect OLED Display pin [VCC] to Arduino pin [5v]

  7. Connect OLED Display pin [GND] to Arduino pin [GND]

Step 3: Start Visuino, and Select the Arduino Board Type

Start Visuino, and Select the Arduino Board Type

Start Visuino, and Select the Arduino Board Type

Start Visuino as shown in the first picture. Click the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Step 4: In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

  1. Add "Debounce Button" component

  2. Add "Digital Multi Source" component

  3. Add "Delay" component

  4. Add "Toggle(T) Flip-Flop" component

  5. Add "OLED I2C" component

  1. Select "Button1" and in the properties window set "Debounce Interval (mS)" to 10

  2. Select "Delay1" and in the properties window set "Interval" to 3000000, you can adjust this by setting any other value

  3. Select "DisplayOLED1" and in the properties window select "Power On" and click on the pin icon and select "Boolean SinkPin"

  4. Double click on "DisplayOLED1" and in the Elements window, drag "Draw Text" to the left side, in the properties window, set "Size" to 3, and "Text" to ARDUINO or any other text

Step 5: In Visuino Connect Components

imageimage

  1. Connect Arduino digital pin[2] to "Button1" pin [In]

  2. Connect "Button1" pin [Out] to "MultiSource1" pin [In]

  3. Connect "MultiSource1" pin [0] to "TFlipFlop1" pin [Set]

  4. Connect "MultiSource1" pin [1] to "Delay1" pin [Start]

  5. Connect "Delay1" pin [Out] to "TFlipFlop1" pin [Reset]

  6. Connect "TFlipFlop1" pin [Out] to "DisplayOLED1" pin [Power On]

  7. Connect "DisplayOLED1" pin [I2C] to Arduino pin [I2C]

Step 6: Generate, Compile, and Upload the Arduino Code

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" Tab, make sure the correct port is selected, then click the "Compile/Build and Upload" button.

Step 7: Play

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project for this tutorial. You can download it and open it in Visuino: https://www.visuino.eu

Download Visuino file: OLED-Auto-Off.visuino

N.º de peça do fabricante 104020208
GRAPHIC DISPLAY MONOCHROME WHITE
Seeed Technology Co., Ltd
N.º de peça do fabricante ST0050
IR OBSTACLE AVOIDANCE SENSOR MOD
SunFounder
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.