Maker.io main logo

Projects Ver tudo

PROJECT
44

Giving Life to an OLD Digit Display

By PTSolns

Exploring a vintage single digit seven segment display with an Arduino Nano Flip. Mapping segments and running counting and chase light modes for fun.

PROJECT
125

Making "The Clapper" Basic Project

By PTSolns

Making "The Clapper", a simple, fun, and quick project that gets you playing with the Nano right away.

PROJECT
234

Changing Bootloader on a Nano using a Custom Shield

By PTSolns

This tutorial shows the steps to change bootloader (old and new) on the Nano development board using a custom shield and an Uno as the programmer.

PROJECT
1.146

Making a Simple RF Network

By PTSolns

A simple getting started project demonstrating one-way RF communication between two nodes using the NRF-Shield.

PROJECT
1.414

Custom 24-Hour Single Revolution Clock

By PTSolns

A custom 24-hour single revolution clock made with an RTC and a stepper motor, controlled by the Nano Flip, all put together on the Proto-Half.

PROJECT
1.220

The Nano That Wanted to Be an Uno

By PTSolns

At the end of the project, you'll get a Nano that has a footprint of the Uno.

Blogs Ver tudo

BLOG
101

Pushing the Limits: A 6km LoRa Range Test with the PTSolns SX1276 Shield

By PTSolns

In this blog, we’ll explore the hardware that’s being used, the science behind the transmission, and just how impressive a feat it is to achieve a 6km range.

BLOG
655

Reversing the Polarity on LiPo Battery JST Connectors

By PTSolns

The 2-Pin JST-PH 2.0 connector is found on many LiPo batteries used in hobby drones, RC cars and toys, and of course, electrical boards and modules. These are handy little connectors, but there is one problem - the polarity convention.

BLOG
4.697

Non-Compliant Use of CH340 V3 Pin: Deep Dive for Engineers

By PTSolns

In this technical post, we explore the widely used CH340 IC from WCH, a popular USB-to-serial converter.

BLOG
124

Measuring the Current Draw on BMP280 Sensor Module

By PTSolns

In this post, we measure the BMP280 barometric pressure sensor in Normal mode and Forced mode using the Nordic Power Profiler Kit II (PPK2).

BLOG
471

Why Your USB-C Cable Won't Program Your Microcontroller

By PTSolns

Not all USB-C cables support data! Some only provide power, causing upload errors on boards like the Nano Flip or ESP32 microWatt. Learn how to spot the difference and test your cables to avoid connection issues in your projects.

Tutorials

TUTORIAL
138

How to Verify the Clock Source on a Nano

By PTSolns

This tutorial shows how to verify the frequency of the clock source on a microcontroller development board. The process is similar for a range of boards, but we will use the popular Nano. This is a good exercise to do as it helps the user get a more in-depth understanding of the Nano microcontroller development board.