Digi-Key Corporation First to Stock NXP LPC11C2x

THIEF RIVER FALLS, Minnesota, USA - março 15, 2011

Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's broadest selection of electronic components available for immediate shipment, today announced it is the first to stock NXP's LPC11C2x series; industry's first integrated CAN microcontroller and transceiver solution.

This new product is now available for purchase on Digi-Key's global websites and will be featured in future print and online catalogs. websites

CAN is recognized as a robust and reliable communication channel for rugged environments. The LPC11C22 and LPC11C24 with integrated high speed CAN physical layer transceiver and easy to use on-chip CANopen drivers offers complete CAN functionality in a low-cost LQFP48 package Typically, CAN transceivers can cost as much as or even more than the microcontroller itself. Integrating the CAN transceiver on board increases system reliability and quality, reduces electrical interconnect and compatibility issues, and reduces board space by over 50 percent while adding less than 20 percent to the MCU cost.

"With the introduction of the LPC11C2x series, NXP now offers seamless integration of CAN into a wide variety of industrial and automation applications for factories, buildings, and the home." said Shelley Unruh, Regional Marketing Manager, Microcontrollers, NXP Semiconductors. "The integrated CAN microcontroller transceiver solution in a unique System-in-Package with on-chip CANOpen drivers extends NXP's plug-and play system approach to help customers save time and cost in their designs."

CANopen drivers are provided in on-chip ROM with easy-to-use APIs enabling users to rapidly adopt the LPC11C22/C24 into embedded networking applications based on the CANopen standard. This standardized layer (EN 50325) is especially well suited for embedded networks in all kinds of control, such as machines and elevators, making proprietary or application-specific application layers obsolete. Incorporating CANopen drivers in on-chip ROM reduces overall risk and effort while providing design engineers with the added advantage of reduced operating power, as well as secure and safe bootloading via CAN.

Digi-Key Corporation focuses on providing customers with superior service, which includes product selection and availability, on-time delivery, and responsiveness. Using leading-edge processes and state-of-the-art technologies, Digi-Key serves a global customer base from its 600,000 square foot facility in Thief River Falls, Minnesota, USA.

About Digi-Key Corporation

Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.