A Framework for Wall-Mount Rack Enclosures in Edge Computing Deployments

By Rakesh Kumar, Ph.D.

Contributed By DigiKey's North American Editors

The edge computing strategy, which moves data processing closer to its source, requires deploying essential IT equipment in non-traditional environments. These locations, such as retail stockrooms, classrooms, and factory floors, pose a primary challenge because they often lack the dedicated floor space, physical security, and climate-controlled conditions of a traditional data center.

Due to these limitations, standard specification criteria are insufficient for the experts responsible for physical deployment. The primary objective of this article is to provide a technical framework for this exact challenge. It describes a technical specification framework that prioritizes serviceability, physical security, and space footprint for these small, uncontrolled areas.

Core challenges in non-traditional IT deployment environments

Edge deployments present three main types of problems, distinct from those encountered during data center construction.

  1. Absence of available floor space: The most immediate constraint in these environments is the absence of dedicated floor space. Most of the time, vertical space is the only available space. As a result, wall-mount solutions are a valuable alternative to traditional floor-standing racks for storing equipment.
  2. Uncontrolled physical security: A data center is a secure facility with controlled access. On the other hand, edge locations are often open to customers, general staff, and students, which poses security risks. In such an environment, an open-frame rack is a liability because it allows network switches, servers, and Uninterruptible Power Supply (UPS) systems to be accidentally disrupted, maliciously tampered with, or stolen.
  3. Uncontrolled environments and access: Edge locations lack consistent service access and dedicated cooling.
    • Climate: There are no cooling systems for these IT deployments. Therefore, dust, ambient air, and temperature changes can affect equipment. The enclosure itself must be capable of managing thermal loads through passive ventilation.
    • Access: When a rack is placed in this manner, non-IT objects may obstruct the service and make it challenging. Longer service times increase the Total Cost of Ownership (TCO) if a technician cannot access the back of the equipment.

The role of wall-mount enclosures as a solution

The suggested solution is to use fully enclosed, locking cabinets rather than open-frame brackets. A simple wall-mount bracket may hold a patch panel, but it fails to solve the core edge challenges. It offers no security, inadequate airflow management, and non-professional cable organization.

Instead, a custom-built wall-mount enclosure works as a standalone micro data center. It is a heavy-duty steel unit that, in a single solution, solves all three challenges:

  • Equipment is moved from the floor to a secure wall.
  • Unauthorized access is prevented via locking steel doors and side panels.
  • Equipment is protected from dust and debris, while airflow is managed via vented panels.

Hence, the selection of such an enclosure is a technical decision that must extend beyond a simple U-height requirement.

A 3-point specification framework for enclosure selection

A successful deployment is dependent on specifying the correct features. These three questions must be answered to avoid common, costly procurement mistakes:

  1. Depth: What is the maximum depth of the deepest component (e.g., a server or UPS) that is to be installed?
  2. Security and access: What are the access control requirements, and who must be prevented from access? How will technicians service the equipment post-installation?
  3. Sizing and load: What is the total required U-space, including room for expansion, and what is the total weight of all components?

Specification point 1: component depth analysis

A common mistake in procurement is failing to verify the component depth against the enclosure's internal specifications. This mistake could stop a deployment if a part is too deep for the chosen cabinet. First, the component with the greatest depth needs to be measured, and an enclosure that fits it needs to be selected.

Wall-mount enclosures are usually grouped by depth.

  • Switch-Depth (Shallow): These are compact enclosures, typically 16.5 inches deep, designed for shallow equipment, such as patch panels and standard network switches. For a simple network drop, a shallow rack such as the Eaton Tripp Lite SmartRack SRW6U, shown in Figure 1, is a suitable choice.

Image of exploded diagram of the Eaton SmartRack SRW6U (click to enlarge)Figure 1: An exploded diagram of the SmartRack SRW6U, a representative Switch-Depth (Shallow) enclosure. (Image source: Eaton)

  • UPS-Depth (Mid-Depth): Depths in this group range from 20.5 to 24.5 inches, making it practical for many uses. This extra space is needed to fit most rack-mount UPS systems and larger Power over Ethernet switches, which are often deeper. Even if the U-height is the same, this difference is still significant. For example, Figure 2 shows the SmartRack SRW18US offering a 20.5-inch depth for switch-heavy deployments, while the SmartRack SRW18USDP extends to 24.5 inches to accommodate the extra room required by UPS systems.

Image of features of the Eaton SmartRack SRW18US wall-mount enclosure (click to enlarge)Figure 2: Key components and features of the SmartRack SRW18US wall-mount enclosure. (Image source: Eaton)

  • Server-Depth (Deep): While many edge deployments do not require servers, this enclosure class is available for those that do. If a deployment requires a 1U server, a "Server-Depth" enclosure is necessary. The SmartRack SRW12US33G (Figure 3), for example, provides a maximum device depth of 32.5 inches, making it one of the few wall-mount solutions that can accommodate 1U servers.

Image of exploded diagram of the Eaton SmartRack SRW12US33G wall-mount enclosure (click to enlarge)Figure 3: An exploded diagram illustrating the components of the SmartRack SRW12US33G wall-mount enclosure. (Image source: Eaton)

Specification point 2: analysis of security, visibility, and service access

After confirming depth, the next consideration is how the equipment will be secured and serviced.

  1. Physical security and compliance: In public areas, the enclosure is the primary physical security measure. All Eaton Tripp Lite enclosures discussed in this article are made of heavy-duty steel and feature doors and side panels that lock. As part of compliance standards like PCI DSS (Payment Card Industry Data Security Standard), this is an important feature that protects physical equipment and media.
  2. Visibility and aesthetics: A solid steel door is secure, but it prevents visual inspection. For this purpose, "G" models, such as the SmartRack SRW12USG, feature a shatter-resistant, clear acrylic front window. Figure 4 shows the model with the acrylic window in the front. This aspect enables at-a-glance monitoring while maintaining a locked state and can help reduce audible fan noise. Additionally, aesthetics are a valid requirement in settings such as clinics and modern offices. In this case, models like the SmartRack SRW6UW in Figure 5 come in a white powder-coat finish to match the surroundings.

Image of Eaton SmartRack SRW12USG enclosureFigure 4: The SmartRack SRW12USG, illustrating the acrylic front window for visual inspection. (Image source: Eaton)

Image of Eaton SmartRack SRW6UW enclosureFigure 5: The SmartRack SRW6UW, demonstrating the white-finish option for aesthetic installations (Image source: Eaton)

  1. Service access and TCO: One of the main factors that affects TCO is how easy it is to service. A static, fixed-back enclosure, such as the SmartRack SRW12U, is initially cheaper to purchase, but it can be challenging to service because technicians often have to remove the equipment from the rack. For a small extra cost, hinged-back cabinets like the SmartRack SRW12US and SRW18USDP (Figure 6) are a better choice. With these models, the entire cabinet body can swing away from the wall, making it easy to access the back panels and cables. This capability can significantly affect service times.

Image of Eaton SmartRack SRW18USDP enlosureFigure 6: The SmartRack SRW18USDP, a hinged-back enclosure specified for its ability to reduce service times and TCO. (Image source: Eaton)

Specification point 3: U-height, weight, and load capacity calculation

Finally, after confirming depth and access requirements, the total size and load must be calculated.

  1. U-Height: A "U" is a standard 1.75-inch unit of vertical space. The total U-height of all current equipment should be calculated. It is recommended to add 25-50% more U-space for future expansion and to improve airflow between components. For 5U of equipment, a 6U rack (e.g., SRW6U) offers minimal expansion space, whereas a 12U rack (e.g., SRW12USG) provides ample room.
  2. Weight and load capacity: The wall must be able to safely support the weight of the enclosure and all the equipment installed inside it.
    • Enclosure Capacity: The rack's load rating must be checked. The SRW6U is rated for 200 lbs, and the larger SRW18USDP is rated for 250 lbs.
    • Wall Integrity: This capacity depends on the quality of the wall's construction. For standard wall-stud placement, all of these enclosures have mounting holes that are 16 inches apart. To keep the enclosure safe, it must be bolted to the building's studs or a suitable concrete structure.

Conclusion

There is no need to sacrifice security, dependability, or serviceability when moving IT infrastructure to edge locations. If an organization uses an objective, facility-focused specification method, it can avoid making common deployment mistakes.

To solve the problem, a custom-built wall-mount enclosure is needed. Organizations can confidently and safely deploy IT infrastructure in any location by following a three-point framework: first, verify the device depth; then, assess the security and access features; and finally, check the U-Height and load capacity. These steps can transform an unusual space into a safe and usable micro data center.

DigiKey logo

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.

About this author

Image of Rakesh Kumar, Ph.D.

Rakesh Kumar, Ph.D.

Rakesh Kumar, Ph.D., is a B2B electronics content writer and strategist and the proprietor of EETips Content Marketing. An IEEE Senior Member and Chair of the IEEE Power Electronics Society Educational Videos Committee, he specializes in creating technical content for electronics manufacturers and distributors. Rakesh has written for WTWH Media publications (EE World, EV Engineering Online), created white papers for TDK Electronics, and contributed to numerous journal and industry publications. With his Ph.D. in electrical engineering, he translates complex technical concepts into clear, practical content that engineers can actually use.

About this publisher

DigiKey's North American Editors