Artigos e blogs

Image of Low-Cost, Power Efficient EMG Prosthetic Hand (Part 2) Low-Cost, Power Efficient EMG Prosthetic Hand (Part 2)

Creating a low-cost prosthetic arm is challenging, but making one that is also easy to calibrate and accurate is even tougher.

Image of Arduino Breakout Boards with IPS TFT Displays for Fast UI Prototyping Arduino Breakout Boards with IPS TFT Displays for Fast UI Prototyping

Arduino‑compatible TFT breakout boards from Newhaven Display simplify prototyping for user interaction with embedded displays.

Image of Piezoelectric Ceramics: Driving the Silent Interaction Revolution Piezoelectric Ceramics: Driving the Silent Interaction Revolution

Piezoelectric ceramic technology generates an electric charge when subjected to mechanical stress and undergoes deformation when an electric field is applied.

Image of Low-Cost, Power Efficient EMG Prosthetic Hand (Part 1) Low-Cost, Power Efficient EMG Prosthetic Hand (Part 1)

Developing prosthetic technology that is both affordable and functional is challenging in today’s space, mainly due to the costly fabrication and specialized calibration requirements.

Image of How to Select Flat-Panel HMIs for Optimal Results in All Industrial Environments How to Select Flat-Panel HMIs for Optimal Results in All Industrial Environments Publish Date: 2026-02-18

Matching the performance of human-machine interface flat-panel displays to requirements in industrial networking applications is complex.

Image of Accelerate Small Display Integration with Plug-and-Play 3.5” IPS HDMI TFTs Accelerate Small Display Integration with Plug-and-Play 3.5” IPS HDMI TFTs Publish Date: 2026-01-15

Designers can now use plug-and-play 3.5" IPS HDMI TFT modules to simplify display integration for industrial and medical applications.

Image of Visualization & Edge Connectivity with Schneider Electric Pro-face™ HMIs Visualization & Edge Connectivity with Schneider Electric Pro-face™ HMIs Publish Date: 2025-12-23

How Schneider Electric’s Pro-face™ HMI portfolio supports automation requirements in packaging, material handling, assembly, and process applications.

Image of The Role of Pulse Width Modulation (PWM) in Electronics The Role of Pulse Width Modulation in Electronics Publish Date: 2025-12-05

A discussion of the basics of Pulse Width Modulation (PWM) as a power-control technique and some of the applications it’s used in.

Image of How to Build a Sample Automation Project in CODESYS How to Build a Sample Automation Project in CODESYS Publish Date: 2025-12-03

Build an automation project in CODESYS, from initial setup to runtime testing by configuring the device tree, mapping I/O channels, programming logic, etc.

Image of Piezoelectric Ceramics: From High-Frequency Compensation to Smart Tactile Feedback, Reshaping Audio and Interaction Piezoelectric Ceramics: From High-Frequency Compensation to Smart Tactile Feedback, Reshaping Audio and Interaction

An innovative application of piezoelectric ceramic earphone units effectively compensates for the shortcomings of traditional dynamic drivers.

Image of Optimizing Industrial HMI Design with Modular 22 mm Pilot Devices Optimizing Industrial HMI Design with Modular 22 mm Pilot Devices Publish Date: 2025-11-05

Explore a modular approach to 22 mm pilot devices that addresses industrial challenges with the Eaton M22 series field-configurable functionality pushbuttons.

Image of Why Rear Enclosures Are Crucial for Miniature Speakers Why Rear Enclosures Are Crucial for Miniature Speakers Publish Date: 2025-10-30

Speakers depend not only on their internal components but also on the acoustic environment in which they operate, such as rear enclosures.

Image of Webinar – Control Panel Solutions: Inside, Outside, and Beyond Webinar – Control Panel Solutions: Inside, Outside, and Beyond

Whether you're designing new panels or retrofitting existing ones, this webinar will help you optimize your layout, boost productivity, and ensure compliance.

Image of Silent Tech Heart: How Piezoelectric Ceramics Drive an Intelligent Future Silent Tech Heart: How Piezoelectric Ceramics Drive an Intelligent Future

Using minimal current, haptic devices can be used to produce precise vibrations. Their ultra-thin profile makes them suited for space-constrained scenarios.

Image of Save Space in Control Panels with Dual-Status LED Indicators Save Space in Control Panels with Dual-Status LED Indicators Publish Date: 2025-08-19

Learn how APEM Dual Icon series LED indicators use dichroic technology to save equipment panel space and provide clear visibility of system status.

Image of Dual Icon LED Panel Indicators Help Designers Improve Clarity Without Complexity Dual Icon LED Panel Indicators Help Designers Improve Clarity Without Complexity

Design efficient status displays using APEM dual icon LEDs. Explore the Q14 Series for smarter, versatile indicator solutions.

Image of Breakthrough in Cost, Vibration Intensity, and Reliability! Breakthrough in Cost, Vibration Intensity, and Reliability!

Add haptic feedback to automotive user control by infusing digital interfaces with tactile logic to give smart cockpits a genuine "tactile language".

Image of Nit Picking the Terms to Describe the Brightness of LEDs Nit Picking the Terms to Describe the Brightness of LEDs

While lumens measure overall light from the device, nits instead measure the intensity of light on a specific area. Valuable to know for display systems.

Image of Behind the Robot: Sensing, Safety, and Control in Industry 4.0 Behind the Robot: Sensing, Safety, and Control in Industry 4.0 Publish Date: 2025-06-19

How sensor, safety solutions and industrial control components contribute to safe motion control, adaptive system behavior, and deterministic decision-making.

Image of Simplifying Panel Design and Safety with TeSys VLS Disconnect Switches Simplifying Panel Design and Safety with TeSys VLS Disconnect Switches Publish Date: 2025-06-18

Industrial infrastructure requires disconnect switches to isolate electrical circuits safely for maintenance, emergency shutdowns, or regulatory compliance.