Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Constant Current Regulators Slide 8

CCRs are self biased transistors that can be two or three terminal devices. The two terminal devices are designed to provide a specific current such as 30 mA. Three terminal devices have adjustable current levels which can be set with an external resistor over a small current range such as 30 mA to 60 mA.

PTM Published on: 2011-11-03